2004-03-10 9:29 PM
2004-03-01 11:46 PM
Hi,
I work on ST10F168 and i use external ram by EBC in 16 bits demux mode. There are 4 Chip Select available for ram : CS1,CS2,CS3,CS4 and 23 adress bits : A1->A23 So, there are (2^23 * 4) bytes accessible <=> 32Mo I would to know if i am right and if i can declare an external memory map of 32 Mo ! Thanks for any suggestions ! Regards, Jim2004-03-02 1:23 AM
Hello Jim,
Unfortunatly the ST10 address range is limited to 16Mo (internal Flash included) because we only use 24 bit to create the total absolute address. Bye2004-03-08 12:35 AM
Ok but 16*8bits or 16M*16bits ?
2004-03-10 9:29 PM
16M*8bits