Posted on May 17, 2011 at 09:49Hi LouisKatorz, Yes, I did the same fix to make works the I2C0. ;-) CAPS is very useful to start a design. It works properly for others functions, but it has to be modified to set I2C. Thanks. BR
Posted on May 17, 2011 at 09:49Hi all, I start a design on STR912FAW44 and I'm using CAPS software to assign pins. But I've a problem to declare I2C0 as master. I2C0 on P2.0 and P2.1. I check registers values generated in conf.h file : :-o #define G...
Posted on May 17, 2011 at 09:49Hi all, I start a design on STR912FAW44 and I'm using CAPS software to assign pins. But I've a problem to declare I2C0 as master. I2C0 on P2.0 and P2.1. I check registers values generated in conf.h file : :-o #define G...
Posted on December 21, 2005 at 10:27Thanks So, NOP are necessary just after changing the state of one port pin direction of a port, or also after changing the value of the port pin ? which NOP are necessary in the example below. Just 1 (or 2) after ...