2008-02-23 7:31 AM
2011-05-17 12:49 AM
Hi,
I finaly pass thrue the interupt process and made it work. This is not an easy way so I try to explain it here. May be this will help another one at his first attemp with the STR9 interupt process. First the doc is not quit clear. I succeed by reading many doc , forum and ask question and a little bit of guessing. Here's what i had to do. I use an external pin p5.6 to generate an interrupt on a REVA board from Raisonance the MCU board is an STR912F. First thing to do is to program the port (5 in my case) in input at least the pin you will use. //GPIO5 init (pin 0-3 N/A) SCU->PRR1 |= 0x00080000; // release P5 reset SCU->PCGR1 |= 0x00080000; // clock gating P5 SCU->GPIOIN[5] |= 0x00; //p5.6 = intr 14(normal input for port 5 pin) GPIO5->DIR = 0x00; // Dir input on GPIO5 for pins 0-7 Second is to understand that the interupt signal pass thrue the wake up unit (WUI) to go in the VIC (Vector interupt controler) so you have to enable it. // Clock for WIU (Enable WIU) SCU->PRR1 |= 0x00002000; // release WIU reset SCU->PCGR1 |= 0x00002000; // clock gating WIU You also have to enable the VIC // Clock for VIC (enable VIC) SCU->PRR0 |= 0x0020; SCU->PCGRO |= 0x0020; The wui will transfert only one pin of the port to the VIc so you have to select it. // Connect Pin P5.6 to VIC1.11 chanel SCU->WKUPSEL &= 0xFFF7; SCU->WKUPSEL |= 0x0030; then you program the adress of the interupt routine in the Vic register // Put the interupt adress in the VAiR 11 register VIC1->VAiR[11] = (unsigned int)&interrupt_handler; note the '&' before the subroutine name now I chose witch interupt IRQ or FIQ it will generate and enable the vic vector VIC1->INTSR &= 0xF7FF; // Generate IRQ instead of FIQ '0' for vic1.11 VIC1->VCiR[11] &= 0xFFC0; VIC1->VCiR[11] |= 0x002B; // enable interupt with vector 11 Then I Finish to program the WUI unit: //program the WIU to transfer interrupt to the vic WIU->PR |= 0xFFFFFFFC; //Clear pendind interupt WIU->CTRL |= 0x02; //Global WIU intr enable WIU->MR |= 0xFFFFFFFC; //Accept external interupt Finaly I enable interup: VIC1->INTER |= 0x0800; // Enable interupt 11 du vic 1 I run the program and when a faling edge on P5.6 pin apend the interupt subroutine is call. Note : on the interup subroutine you have to clear the interupt void interrupt_handler (void) { //dummy code count++; WIU->PR |= 0xFFFFFFFC; //Clear pendind interupt VIC1->VAR = 0; // Clear interupt } I hope that will help some of new one with STR9. If you have any comment and some explanation please do so Thank you Mike 8-)2011-05-17 12:49 AM
I try to use external pin P5.6 to generate an interup but the interupt never apend.
I use REVA board with STR912F MCU I'm working in debug Here my code: #include ''STRx.h'' int delaycnt; int k; void interrupt_handler (void); ... ... function ... ... void interrupt_handler (void) { int i,l; i=1; l=i; VIC1->VAR = 0; } int main() { int i; int status = 0; int cote = 0; int size = 0; int suivant = 0; int timerst = 0; int timerval = 0; int timerval2 = 0; float volt; mg=0; //init device initcpu(); //initialise GPI0 0 to 9 // Interupt init // Clock for VIC SCU->PRR0 |= 0x0020; SCU->PCGRO |= 0x0020; // Connect Pin P5.6 to the external interupt 1 SCU->WKUPSEL &= 0xFFF7; SCU->WKUPSEL |= 0x0030; VIC1->VAiR[11] = (unsigned int)interrupt_handler; VIC1->VCiR[11] = 0x20; // enable interupt vector VIC1->VCiR[11] |= 0x0B; // specify interupt number VIC1->INTSR = 0x0000; // Generate IRQ instead of FIQ VIC1->INTER = 0x0800; // Enable interupt 11 du vic 1 VIC1->VAR = 0; // Acknowledge Interrupt do { i =2; } while (i = 2); ... code ... } The port 5 is put in input modes as follow: //GPIO5 init (pin 0-3 N/A) SCU->PRR1 |= 0x00080000; // release P5 reset SCU->PCGR1 |= 0x00080000; // clock gating P5 SCU->GPIOIN[5] |= 0x00; //P5.6 = intr 14 default GPIO5->DIR = 0x00; // Dir input on GPIO5 for pins 0-7 I put a breakpoint in the interupt code but it never hapend. What is wrong. It should work ??????? help please Mike2011-05-17 12:49 AM
Bonjour Michel,
I worked out a similar config. But there is something that really bothers me: as soon as I recover GPIO5 from reset and enable clocking, all pins but 5.3 switch to ''High''. I have the Keil MCBSTR9 with STR912FAW using uVision3. Even when I change the status manually via the Peripheral menu, it changes back the very next pulse. Actually, an interrupt is not really needed for my application. All there is to be done is check, whether a switch is closed or not: P5.6 (output set to 1) -----/ ----- P5.7 (input) Now my programme checks the status of 5.7. But due to the problem mentioned above, the pin is always high... Does anyone have an idea on this? Cheers Nik2011-05-17 12:49 AM
I still work on my interup software and I have some more info to share.
As far as i know, pin of port 5 will be conect to the vic 1.11 port 6 to vic 1.12 port 7 - vic 1.13 and port 3 to vic 1.10. It means that only one pin of each port is available for interup in a moment. It's possible to chose the Rising or falling edge of the interupt signal in writing on the WUI_TR register. WIU->TR |= 0x0000; //triger polarity 0 falling 1 rising it is possible to change the priority of each interup routine with the VICx_VCiR[xx] number but I don't know exactly how it's work. I made some experiment but I dont have any sure conclusion VIC1->VCiR[11] |= 0x002B; // enable interupt with vector 11 VIC1->VCiR[11] |= 0x002A; // enable interupt with vector 10 If someone could explain I'll apreciate. Also why is there 5 bit in the VCiR register to select the interup source 4 had been enough? In my program I made general programation by it could be more specific ex: WIU->MR |= 0xFFFFFFFC; //Accept external interupt you could be more precise ex WIU->MR |= 0x000010C; If someone have more detail please do so. We will apreciate your help. Mike 8-)2011-05-17 12:49 AM
I already meet this problem. I was working with Ride ver 6.0. As soon as i put the pin in output mode with the command (SCU->GPIOOUT[5] |= 0x5555;)i couln't return it to input mode SCU->GPIOOUT[5] |= 0x0000. I send a request to technical support but didn't find any answer. I install the version 7 of ride software and the problem disapear for the 2 version. I couln't explain it. May be there was a bad driver...
Hope this will help you2011-05-17 12:49 AM
Hi Michel,
I only want to show you a little misstake. If you code SCU->GPIOOUT[5] |= 0x5555; and try to reset it with SCU->GPIOOUT[5] |= 0x0000; this won't work because you use the OR | Operator. ex: 1|0=1 If you want to reset it, use SCU->GPIOOUT[5] = 0x0000; If you only want to reset Pin 0, use SCU->GPIOOUT[5] &= ~0x0003; I hope this can help you. If not, keep on trying.