2024-10-31 2:01 PM
Hi,
any help or information to find the data sheet and to determine an available replacement type for an obsolete EEPROM chip from ST marked 950406 would be highly appreciated.
A picture of the chip is attached.
The defective EEPROM chip 950406 comes from a Landis & Staefa heating controller, year of manufacture of the controller was +- 2002.
Thanks in advance and best regards.
2024-10-31 2:43 PM
ST95040M6TR SOP8
EEPROM 5.5V 4K (512x8)
2024-11-01 1:28 AM
@Tom6 You could try the M95040-RMN6TP or the M95040-FMN6TP. The ST950406 can only be operated with 5V, but the alternatives can be operated from 1.7V or 1.8V up to and including 5V.
Hope that helps?
Good luck!
/Peter