cancel
Showing results for 
Search instead for 
Did you mean: 

Cooling surface HiP247-4 package

schenkpa
Associate

Hello, i am using the SCTWA60N120G2-4 for a traction inverter. It has a HiP247-4 package and of course needs to be cooled. I did not find any information saying that the cooling surface of the package ist isolated or not isolated. Is there any information, which i was maybe not able to find, regarding the isolation of the cooling surface of the package? 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @schenkpa, to the community!

The data sheet of the SCTWA60N120G2-4 shows the pinout of the SiC MOSFET on the first page, which also contains Drain(1, TAB). Here, 1 stands for pin 1 and TAB for the metallic back of the HiP247-4. The TAB is therefore not isolated.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.