2022-10-18 06:17 AM
I have a circuit with 2 L5983TR on it. On his generating a 3.3V supply the other 1.2V. 1.2V supply is fine, but the 3.3V supply is switching off. Circuit was generated using DesignSuite, and I have changed pretty much every component but to no avail. Current draw is about 200mA. Time for the scope trace is about 10 seconds.
2022-10-21 06:52 AM
Hi @Community member ,
first of all thanks for your interest in our product and for using eDesignSuite for your application!
From the schematic we can't understand if it can be a problem due to an incorrect layout or if the regulator reaches the current limit.
Please, be sure that:
Let us know if all these conditions are verified, so in case we can go in a deeper analysis.
Thanks,
Patrizia