2024-09-29 12:12 PM
When I try to install it I get this error: "The following packages have unmet dependencies:
st-stm32cubeide-1.16.1 : Depends: libncurses5 but is not installable
Depends: libpython2.7 but is not installable
Depends: libwebkit2gtk-4.0-37 but is not installable"
any ideas? thanks in advance
Solved! Go to Solution.
2024-09-29 04:44 PM
Hi,
These are my notes for installing CubeIDE onto Tumbleweed -
STM32CubeDE installation
Download the generic linux option. The RPM package is problematic!
DON'T use the sudo running the script.
Select NO to install stlink server.
Using sudo & kate, create a desktop file in "/usr/share/applications/st-stm32cubeide-version.desktop". You need to logout - login to finialise it.
Before launching, create the workspace folders required. Copy/ move the projects from the old workspace to the new one.
When launching, select the new workspace, then import the project(s).
I hope this helps.
Kind regards
Pedro
2024-09-29 12:36 PM
Which version you try? -> try : generic Linux...
2024-09-29 01:20 PM
I tried it and it gives the same error
2024-09-29 04:44 PM
Hi,
These are my notes for installing CubeIDE onto Tumbleweed -
STM32CubeDE installation
Download the generic linux option. The RPM package is problematic!
DON'T use the sudo running the script.
Select NO to install stlink server.
Using sudo & kate, create a desktop file in "/usr/share/applications/st-stm32cubeide-version.desktop". You need to logout - login to finialise it.
Before launching, create the workspace folders required. Copy/ move the projects from the old workspace to the new one.
When launching, select the new workspace, then import the project(s).
I hope this helps.
Kind regards
Pedro
2024-09-29 05:06 PM
I will try, thanks in advance