You can find my simulation in the attached file
Hi, I am an Electrical Engineering Student in France (at INSA Lyon) and I am in an Electrotechnical club. We have built a Tesla Coil and we drive it using IGBTs (H-Bridge/4 IGBTs) but we have an issue with the frequency and the current (too high / ou...
TS3011 pspice file posted on the ST website cannot translate to ADS. The file shows ten pin circuits after translation, while the device only has five pins
I'm trying to activate all constellation on my Teseo-LIV3FL module and then it says Glonass and BeiDou constellations aren't supported at the same time, but why? The docummentation didn't explain any further about this issue.
Good day, Support TeamI'm working on a single-phase Panel meter. Which provides import and export of both energy sources on ModbusFor metering purposes, we are considering the STPM3x family of ICs (STPM32, STPM33, STPM34).I've attached one image from...
Below is a screenshot from Teseo-Suite for my Teseo-LIV3FL GNSS ModuleLighter flag color means the satellite is not used. As you can see GPS satellite with PRN 16 has higher SNR (23dB) than PRN 9 (21dB) which means the signal quality should be better...
The square antenna inductance equations in app notes AN2972 and AN2866 seem to contain an error (or misleading terms) where it describes the average diameter parameter. The notes say the average diameter in millimeters but it needs to be in meters in...