cancel
Showing results for 
Search instead for 
Did you mean: 

I need help with the TS3011 comparator pspice file to be translated to ADS format.

RA2
Associate

TS3011 pspice file posted on the ST website cannot translate to ADS. The file shows ten pin circuits after translation, while the device only has five pins

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @RA2​, to the community!

You unfortunately had a typo and I took the liberty of changing the device name to the correct TS3011 if that's OK with you?

Sorry you are having problems with the conversion. However, this seems to be a problem of ADS, because in the SPICE model only 5 pins are clearly mentioned:

************ CONNECTIONS: 
****             NON-INVERTING INPUT
****              |  INVERTING INPUT
****              |   |   POSITIVE POWER SUPPLY
****              |   |    |   NEGATIVE POWER SUPPLY
****              |   |    |    |  OUTPUT  
****              |   |    |    |   |     
****              |   |    |    |   |  
.SUBCKT TS3011   VP  VM  VCCP VCCN  VS

Maybe Keysight Technologies support can help you? 

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.