Other: software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Copy & Paste for component values

Posted on January 30, 2015 at 19:05Is it possible to make fields with component values e.g. capacitors, copyable (e.g. via mouse right click) in eDesignSuite so they can be pasted into other documents or distributors search engines.  This would elim...

robin2 by Associate
  • 289 Views
  • 1 replies
  • 0 kudos

Spice model for power factor controller L6563s

Posted on December 19, 2014 at 16:57Dear friends,  I am in need of Pspice model for power factor controller L6563.please post ur suggestion for getting the same or is any other way to simulate the power factor correction? #spice-model #l6563h #l6...

rachid2 by Associate
  • 407 Views
  • 0 replies
  • 0 kudos

ESM7045DV datasheets

Posted on November 09, 2014 at 03:21Dear all, I had been trying really very hard to search by internet and or trying to call ST distributor searching for DATASHEETS of ESM7045DV, unfortunately I found nothing.Is there anyone that could help me out p...

AC/DC Transformer help

Posted on April 17, 2014 at 19:55Wurth has ready transformers for AC/DC supplies for 12V, 24V and 48V for 150W, 200W and 250W ratings. The details can be found here: http://katalog.we-online.de/en/pbs/WE-LLCR?sid=f6723a16ca Can these be used readily...

ravindra by Associate II
  • 322 Views
  • 1 replies
  • 0 kudos

PM6680A based project simulation in eDesign Studio

Posted on March 27, 2014 at 14:531) After saving either locally or remotely the project, I can't find anymore my database added components. Could it be wanted or a bug? 2) PSpice export option is grayed, is it because ST PSpice Project Export Manage...

olmirko by Associate
  • 385 Views
  • 1 replies
  • 0 kudos

Problem with L6566BH wide range input (90-400Vac)

Posted on August 22, 2013 at 15:08Hi We used eDesignSuit. The Vin is designed from 90Vac to 400Vac (phase-neutral or phase-phase)  and the Vout is 16V, 1.3A (max) (about 21W), in QR mode with fmin 150kHz and Fmax 300kHz. If we supply the circuit wit...

STGIPL14K60

Posted on July 19, 2013 at 06:07I bought STGIPL14K60 ..I want to rectify the 3 phase input. When i rectify it , I got about 585VDC.  Can i connect this high voltage to the MODULE or not. #edesignsuite #pfc #power-supply #rectifer #dc-chopping #s...

0690X00000605dMQAQ.png

VIPer17

Posted on July 12, 2013 at 18:56Hello,I have design Led driver of VIPer17LN with eDesignSuite.In put AC 230V   o/p 22V .35A (Led 3.2v 350ma x 7)But could not find EMI component value in BOM.Also the value of Cin is 0 F.Please help.Ravi.