2024-11-09 11:54 AM - last edited on 2024-11-11 08:45 AM by Andrew Neil
i need help with a project, mainly wiring diagram and other information. I have sent components images
i need to wire up two stm32f103c8t6 to
1. 5 4-pin tact switch
2. 3 5-way tactile switch
3. 5 3-way toggle switch (6-pin)
4. 2 wh148 10k potentiometer with knob
5. 1 ps2 joystick module breakout sensors (5v, push button when pressed down, Rx-Ry)
6. 4 ss49e analog hall effect sensor
7.10pF 50v ceramic capacitors dip ( please tell me how many to use )
8. 1N4148 1W zener diode
I will need to make all this wired up on first stm32f103c8t6
and on the second stm32f103c8t6 i need to wire these components
1. 4 4-pin kd4-22n push button switch dpst with lamp
2. 4 4-pin rocker switch with lamp
3. 8 3-pin 2 way toggle switch
4. 2 a10k potentiometer 3-pin
5. 1 100k potentiometer 3-pin
this is my first stm32 project soo any additional information will be very useful
Thanks You
2024-11-09 11:58 AM
also can the tactile switch be used as button matrix
2024-11-11 08:52 AM
@kalpaknirale wrote:i need help with a project, mainly wiring diagram and other information.
Are these not part of your project - ie things that you need to do?
Are you designing your own boards, or using ready-made?
Even if you will eventually be designing boards, you should start on development boards to prove your design.
NUCLEO-F103RB should be suitable:
https://www.st.com/en/evaluation-tools/nucleo-f103rb.html
Schematics are available on the 'CAD Resources' tab:
https://www.st.com/en/evaluation-tools/nucleo-f103rb.html#cad-resources
You can see examples of using switches there...
If designing boards, study AN2586, Getting started with STM32F10xxx hardware development:
Also take a look at the other Application Notes available on the Product Page:
https://www.st.com/en/microcontrollers-microprocessors/stm32f103rb.html#documentation