2022-06-08 02:31 AM
I want to use the WiFi module
IDW01M1 and/or IDW04A1. In both quick-Start-Guides I get the tip to download the "X-Cube-WiFi1 expansion software package for STM32Cube". Unfortunately all the Links for this file are broken/dead.
Is this package compatible with the newest CubeMx? Is the middleware in other cube files integrated?
Thanks in advance
Christian
Solved! Go to Solution.
2022-06-08 11:06 PM
The software package was called X-CUBE-WIFI1 and was applicable for SPWF01SA and SPWF04SA. It is also obsolete and thus no longer available from STMicroelectronics.
But maybe you can still find it in the depths of the never forgetting internet?
Good luck!
If the problem is answered, please mark this topic by selecting Select as best. This will help other users find that answer faster.
/Peter
2022-06-08 05:07 AM
Welcome, @Community member, to the community!
These were X-NUCLEO boards that served as development kits. On the X-NUCLEO-IDW01M1 was the module SPWF01SA, while on the X-NUCLEO-IDW04A1 was the module SPWF04SA.
It is important to note that both WiFi modules have long since been discontinued and there is therefore no longer any support for the modules.
The expansion software was also not installable in STM32CubeMX, but one used the drivers and sample programs directly or integrated them manually into one's project.
Does it answer your question?
Regards
/Peter
2022-06-08 09:32 PM
Hello Peter,
thanks for the response. I know that the modules are discontinued. But I got lot of them (modules and X-Nucleo boards) and I thought, that I can use them for some WiFi projects. So it would be nice to get the X-Cube-WiFi expansion software package as a starting point.
So my question is:"Is there a way to get this expansion software package?"
Regards
Christian
2022-06-08 11:06 PM
The software package was called X-CUBE-WIFI1 and was applicable for SPWF01SA and SPWF04SA. It is also obsolete and thus no longer available from STMicroelectronics.
But maybe you can still find it in the depths of the never forgetting internet?
Good luck!
If the problem is answered, please mark this topic by selecting Select as best. This will help other users find that answer faster.
/Peter