2020-03-16 01:52 AM
The EEPROM M95512-D has an identification page that could be write protected permanently. In teh datashett is the address of this page not mentioned. I need to know the address for the identification page.
2020-03-16 03:01 AM
2020-03-16 03:08 AM
Hello,
i want to read/write the identification page, but in table 5 is only given A6 to A0? What is the starting address for the identification page?
The memory map in figure 4 shows the identification page behind the EEPROM area, so the address should be higher that FFFFh, but that
is not possible. Means either table 5 or figure 4 is wrong
Thx
2020-03-16 03:20 AM
Ok I understand now your concern.
In fact the identification page starting address is 0x00 and you have 128bytes available .So 7 bits ( A6 to A0 ).
BR
2020-03-16 03:25 AM
Oh, yes, now i understood.
Thank you very much for the quick support, case can be closed.