cancel
Showing results for 
Search instead for 
Did you mean: 

VNF1048F device is in LOCKED state always

krishnaduriseti
Associate

Hello Team,

I have some problem with unlocking the VNF1048F chip using SPI communication, I have the got the read working but chip is always in LOCKED state and when I try to unlock according the sequence mentioned in datasheet doesn't work.

I try to set UNLOCK BIT , WD_TIME and WD_TRIG bits in CR3 and in the next step

I try to set EN bit in CR1

But when iIread back these registers, values are 0 always and status register (0x11) shows LOCKEDM is 1 WD_FAIL is 1. To be able to set WD_TIME and WD_TRIG bits should I unlock the device first?  Not sure what is the startup sequence.

Could you please share the initial configuration of the chip or any example code would be greatly appreciated.

Thank you in advance !!

Regards,

Krishna duriseti.

1 REPLY 1
krishnaduriseti
Associate

Hello Team,

Do you have any feedback for my post. As this is bit critical for our Project, Any feedback is greatly appreciated.

Thank you so much and looking forward for your feedback,

 

Regards,

Krishna.