2007-05-13 09:35 PM
2011-05-17 12:43 AM
The DFU project provided in the UM0290 doesn’t work on the STR910 EVAL board. I'm trying to debug the application for IAR using this project and haven’t had any success. When I try to debug this application, the debugger stops at the following initialization in the 91x_vect.s file:
IMPORT Undefined_Handler The hex file generated from this project doesn’t work either when downloaded using the CAPS tool. Is there any manual for this DFU project? Any help in this regard would be appreciated.