2005-01-06 09:42 PM
USB code for uPSD3254A needed - Urgent
2011-05-17 03:05 AM
Hi all,
I have a problem in USB. I am using uPSD3254A device and I tried the sample demo application for USB (with windows application) from the STMicroElectronics site. After powering up the board, when I say connect from the windows application (given by ST) it says ''Failed to connect to ST demo board''. Can you provide me the USB code that is running on the uPSD3254A device. Or should I do any modification onto the demo code before downloading into the chip. Please help me to solve this problem. Thanks & Regards, Hariharan