2004-09-23 05:33 PM
uPSD Sound Studio and uPSD32xx/uPSD33xx Setup
2011-05-17 03:03 AM
We are interested doing sound generation using uPSD33xx as noted in Application note AN2007.
Question 1: Where do you download the uPSD Sound Studio V1.0 application? Question 2: The application note example used the 8 pages of main flash memory (fs0-fs7). If we expanded the number of pages using external flash, can the uPSD Sound Studio handle these extra pages when creating the final HEX files for the PSD Soft Express utility? The uPSD Sound Studio application appears to work only with uncompressed .WAV files. The 256K main flash is limited for our needs but if we add the maximum addressable flash externally we'd have more than enough.2011-05-17 03:03 AM
Please send your questions to the application engineering department at:
mailto:apps.psd@st.com
. Also provide the following information so we can better help you: Name Company Name Phone Number Location (City, State, Country) Production uPSD part number (3234, 3334, etc.) Application Projected annual volume (units) Production start date Thanks, uPSD Applications Engineering