2006-02-25 05:39 PM
Time to stabilize internal oscillator
2006-02-25 05:39 PM
Hello,
I am using ST10F269-Q3 with custom power supply, which generates RESET signal for MCU. I found in ST10 datasheet, p.103, phrase: ''Depending on crystal frequency, the on-chip oscillator needs about 10ms to 50ms to stabilize.'' So can you say what delay must be enough between VDD valid (> 4.5 V) and RESET up ? I am using crystal MG3A connected to ST10 with two NPO capacitors 22 pF on GND. Crystal frequency 10 MHz, multiplier = 4. Is there any formula, table or another rule to select this time delay ? Thank you.