2003-09-18 04:33 AM
Strap options for CPU Clock Multiplication (486 mode) - Atlas
2003-09-10 11:19 AM
Hi,
What happens if you have MD[14] = 0 and MD[40] = 1 on an Atlas? The datasheet indicates that this is a reserved setting. Any idea of what this reserved setting does and what speed the system will run at? Can it be used with HCLK = 66 MHz?2003-09-16 09:53 PM
Hello,
The settings that you describe is for x3 mode but it cannot be used with HCLK=66MHz.2003-09-18 04:33 AM
Please be advized that the STPC Atlas does not support these multiplication factors and if they are selected will not be work reliably.