Posted on September 10, 2003 at 20:19Hi, What happens if you have MD[14] = 0 and MD[40] = 1 on an Atlas? The datasheet indicates that this is a reserved setting. Any idea of what this reserved setting does and what speed the system will run at? Can...
Posted on January 30, 2003 at 14:40Thanks. Do you know the maximum transfer rate on it for an HCLK of 100 MHz? The timing diagrams for the local bus don't seem to indicate how long you wait after the cycle is complete to when another cycle starts, s...
Posted on January 27, 2003 at 18:05In the STPC Elite programming manual it says that ISA 16 bit bus cycles are 2.5 clocks long. This seems very low to me. In addition, I can't seem to be able to find how frequently ISA bus cycles are executed. On mo...