Posted on February 22, 2007 at 11:54Hello, Each devices can be put on each bank. The size for (each bank) is limited at 16MB. The chip select signals will be different for each devices and they will share the same data bus, address bus and read/writ...
Posted on January 04, 2007 at 13:41Hello, If I understand well, 3 kind of devices will share the EMI data bus which are RAM, printer and LCD. And you will select these devices by using nCS0 and buffer_en signals. The same EMI bank for the devices. A...
Posted on December 19, 2006 at 05:46Hello, This solution should not work because when the CS signal is not asserted, the data bus will be Hi-Z. If you use other signals than EMI ones to drive the LCD, maybe it could work. Another problem is the EMI ...
Posted on August 31, 2006 at 09:21Hello, The address 0 is not used on the STR71x eval board schematic because 2 x 2M x 8bit are used. And 2 x 2M x 8bit is the same as 2M x 16bit. And with 16 bit memory on EMI, the A0 is useless. If you want to map o...
Posted on June 29, 2006 at 10:21Hello, If your Core CLK is 36 MHz and if you want a 250K bit rate for the CAN0. Please do the following after the initialization: CAN_EnterInitMode(CAN0, CAN_CR_CCE); CAN_SetTiming(CAN0, 11, 4, 4, 9); CAN_LeaveInitMod...