2006-10-23 05:11 AM
STR9 FreeRTOS port with WEB server
2011-05-17 12:30 AM
Hi,
I hope it might be of interest that the latest FreeRTOS.org download includes an STR912 port with a WEB server demo. The ENET driver has been extended from that available from the ST site to make full use of the DMA on the Rx and (hopefully) auto negotiate the protocol. See for more info. Regards, Richard.2011-05-17 12:30 AM
Hi,
I can't open the link, what's wrong? Thanks.2011-05-17 12:30 AM
I just tired clicking it an it seems fine. Try going directly to
. I know the site is not accessible from within China, so if that is where you are based there is not much I can do about it I'm afraid :-(2011-05-17 12:30 AM
I should have mentioned you can still get the source code even from within China,
but might be tricky without the documentation. The STR9 demo project for IAR is in the Demo/ARM9_STR91X_IAR directory.2011-05-17 12:30 AM
Thanks so much. I am going to try it on the STR912 board.
2011-05-17 12:30 AM
Hi,
I looking into porting FreeRTOS on this Micro using the Keil tool. Please help me with a good starting point Thanks2011-05-17 12:30 AM
Hi,
I looking into porting FreeRTOS on this Micro using the Keil tool. Please help me with a good starting point Thanks2011-05-17 12:30 AM
Hi,
I looking into porting FreeRTOS on this Micro using the Keil tool. Please help me with a good starting point Thanks2011-05-17 12:30 AM
See the following link:
https://sourceforge.net/forum/message.php?msg_id=3835217