2005-03-16 02:12 AM
2005-03-14 08:30 AM
The ST720 has 16K on-chip SRAM. But in the data sheet, the SRAM is always referred to as “program RAM�. In section 6.1, the data sheet states that “Program Memory can be used for both code (instructions) and data (constants, tables, etc.) storage.�
Does this mean that there are certain restrictions when the on-chip memory is data storage (such as read-only, and unit of access (e.g 32-bit boundary only), etc). We want to make certain that the on-chip SRAM can be read and written in byte, word (16 bit) and long word (32 bit) units to store frequently accessed parameters. Can you verify this for us?2005-03-14 08:13 PM
Hello bugaloo,
Can you tell me which revision of the datasheet and reference manual you use. I think you have an oldest one, you find the new revisi on in the web site. Best regards, Hich ;)2005-03-16 02:12 AM
Good morning,
The STR720 datasheet I am using is the Dec 2004 version 4.0. is there a more recent one??? Regards, Terry