Posted on May 17, 2011 at 09:33Good day, Problem Statement: I cannot get SSP0 (Master)to communicate properly with SSP1 (Slave), similar to your SSP code Example1. 1) The serial data on the MISO line (using a logic analyzer) is ''CORRECT''. But when...
Posted on August 18, 2006 at 18:04 can not get the I2C 0 Serial Port on the STR712F to work properly. I'm trying to use the I2C 0 in Master Transmit Mode using the C code below => exactly as described on pages 213 through 216 of the STR712F Refere...
Posted on March 16, 2005 at 11:12Good morning, The STR720 datasheet I am using is the Dec 2004 version 4.0. is there a more recent one??? Regards, Terry
Posted on March 14, 2005 at 17:30The ST720 has 16K on-chip SRAM. But in the data sheet, the SRAM is always referred to as “program RAM�. In section 6.1, the data sheet states that “Program Memory can be used for both code (instructions) and da...