2007-12-07 01:11 AM
STR712FR2: problems with interrupts while running from RAM...
2007-12-03 10:41 PM
Dear All,
I have encounered a problems with interrupts while running code from RAM... Environment: Keil uVision 3.55a and MDK 3.15b I took an example from Examples\ST\STR71xLib\Tim\OCMP and changed it in the way to work in RAM. What i see is that Timer 3 output compare function pin triggers but interrupt routine doesn't work (there are no port pins toggling)... When i run it in debug mode (using the internal uVision debugger) all seems to be working... Does anybody encounter with such problems before? I would be very appreciated for your help. P.S.Source code i'm experimenting with is attached for your consideration... Thank you. ________________ Attachments : OCMP.ZIP : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1NS&d=%2Fa%2F0X0000000bmC%2FqFJqRlnvhC9zyQOZAYNG8KIfJK7mU4OgE2s.E_r4d7Q&asPdf=false2007-12-07 01:11 AM
I have an STR710 interrupt example running from RAM and the porject setting is different than yours. you can check also the boot pin on your board. I attached my setting. Hope this helps you,
Cheers, Chris. [ This message was edited by: christophe.beyen on 07-12-2007 14:43 ] ________________ Attachments : project-setting.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtQZ&d=%2Fa%2F0X0000000aPs%2Fmnzo5O4R9sLjnD3M8kBe.y98FobZG6VD6elw6H1kIUQ&asPdf=false