cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL STRKT01

hassanmaree
Associate II

Hi I am a new user, Can any please tell me which software do I need to use for STEVAl STRKT01? My aim is to transmit lora signal and received this signal on spectrum analyzer.

10 REPLIES 10
Andrew Neil
Evangelist III

Yes, I have checked the documents. It does not tell about which software to use to access the device. 

Your read the UM2541 User Manual ?

And looked on the 'Software' tab?

AndrewNeil_0-1714402147794.png

 

AndrewNeil_1-1714402287462.png

 

hassanmaree
Associate II

Thank you very much, I will try to use this software. 

hassanmaree
Associate II

Does it have any hardware driver?

 

Read the User Manual UM2487Getting started with the STM32Cube function pack for IoT tracker node with LoRa® connectivity, GNSS and sensors

Hi Andrew, 

I am trying to change device join parameters using serial communication via Putty. It doesnot get changed

hassanmaree
Associate II

I have updated my firmware of STEVAL-STRKT01 using st nucleo board. The firmware is a binary file file with location {en.fp-atr-lora\STM32CubeFunctionPack_LORA1_V2.2.0\Projects\STEVAL-STRKT01\Applications\LoRa\Asset_Tracker\Binary\STEVAL_STRKT01_EU868.bin}

I have access the module using putty.

The output in putty is 


ST Microelectronics
LoRa Smart Tracker firmware
APP_VERSION= 01.03.00.00
MAC_VERSION= 04.04.02.00
LoRa IOT tracker app version: 2.2.0
Battery voltage 0.00 V
Battery charge: 0%
Charger status 9
BATTERY_TEMP_FAULT_OR_NOT_PRESENT
Got sensor data: T: 28.15 H: 50.77 P: 1014.20
Accelerometer: X: 25 Y: -61 Z: -976
Got coordinates: 52.764061 N, 1.242864 W, ALT:110.160004
19/11/20 16:00:57 - 0 sats - Fix 0
Battery voltage 0.00 V
Battery charge: 0%
Charger status 9
BATTERY_TEMP_FAULT_OR_NOT_PRESENT

Processing command: ?devicejoinparam

DevEui(FromMcuId) = 32 37 32 38 4C 37 7B 08
Application uses the Over-the-Air activation procedure.
Active keys:
DevEui = 32 37 32 38 4C 37 7B 02
JoinEui = 01 02 03 04 05 06 07 08
AppKey = 5F 06 5A 8B 60 5A 0C 2E 12 3C E1 30 5D 53 28 E4
NwkKey = 5F 06 5A 8B 60 5A 0C 2E 12 3C E1 30 5D 53 28 E4

ADR: N, DATA RATE: DR_4, PUBLIC NETWORK: Y
Command complete

I have registered this on ttn network as well. image attached.

hassanmaree_0-1720722019874.png