2003-07-03 04:05 AM
2003-07-01 05:38 AM
St7lite2
I have a problem with ‘current’ on the ST7lite2 during the first 30 seconds after a reset. Too save ‘current’ I’m switching from slow to fast mode using an interrupt, which works OK. The problem is that during the first 29 second after a reset, the current slowly rises and then drops and then will stay consistent thereafter. Any ideas?2003-07-01 09:47 PM
Hi
Are you sure this is the micro and not due to external components. Are you using your own target system or an evaluation board from Softec etc? Simon2003-07-01 09:51 PM
Using own target board.
Works ok using a ST216 instead with the same code on2003-07-01 11:10 PM
Hi,
Sorry, another question - Is that with the '216 used on the same target using an adapter? or the '216 on a different target board? Thanks, Simon2003-07-03 04:05 AM
I've sorted the problem
I had an unsed Port A (HS) configured as an input. Changing it to a output has solved the problem I'm still looking at ways of getting around the current used by the LVD on.