2007-04-24 08:50 AM
ST7 Programmer - Illegal System DLL relocation
2007-04-12 03:29 AM
I noticed today after recently changeing over from the IDEA (Cosmic IDE) to ST7 Visual Develop. I am getting an error when running the ST7 programmer:
stvp.exe - Illegal System DLL Relocation The system DLL user32.dll was relocated in memory. The application will not run properly. The relocation occurred because the DLL C:\Windows\system32\HHCTRL.OCX occupied an address range reserved for Windows system DLLs. The vendor supplying the DLL should be contacted for a new DLL. I'm not sure if this is related to HHCTRL.OCX but was wondering if anyone else has had the same problem?2007-04-12 03:44 AM
Hi,
This has been yet reported and it is related to a Microsoft update : The problem doesn't come from STVP7 but from the windows update Microsoft has fixed the problem: ==> Best regards Laurent2007-04-24 08:50 AM
Thanks for the information, I was starting to panic. MS wasn't much help until you displayed the link.
Thanks Dave P :D