cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F252 details

sreeram
Associate II
Posted on March 17, 2006 at 05:05

ST10F252 details

3 REPLIES 3
sreeram
Associate II
Posted on March 07, 2006 at 02:23

Hello,

Does any body know some details about the CPU ST10 F252 - like part number, evaluation kit details etc..? I could not find it in the website. It is similar to F269 with 256K Flash and 20k RAM.

najoua
Associate II
Posted on March 07, 2006 at 04:22

Hello,

The ST10F252 is a new derivative of the STMicroelectronics ST10 family of 16-bit single-chip CMOS microcontrollers. It combines high CPU performance (up to 24 million instructions per second) with high peripheral functionality and enhanced IO-capabilities. It

also provides on-chip high-speed single voltage FLASH memory, on-chip high-speed RAM, and clock generation via PLL.

It is built using a 0.18 μm CMOSM8 process, with 1.8V internal core logic voltage, but 5.0V IOs and a single 5.0V supply voltage. The device implements an on-chip voltage regulator for the core logic supply.

Third parties supporting this MCU:

- PLS is a software tool provider

- Phytec provides an eval board based on the ST10F252. You can contact them for more details.

I hope this helps,

Regards,

Najoua.

[ This message was edited by: Najoua on 07-03-2006 09:12 ]

sreeram
Associate II
Posted on March 17, 2006 at 05:05

Thanks a lot for the info..

I have some more questions.

We have a Dprobe ST10 emulator from HITEX for ST10F275/276/269. Can I use it for debugging ST10F252 with some minor upgrade? If so what exactly should I do to upgrade the emulator?

Are there any other debug hardware available for ST10F252? I think Lauterbach has an emulator called FIRE ( Fully integrated RISC Emulator) which supports this processor, but that is quite expensive.

Any suggestions?