cancel
Showing results for 
Search instead for 
Did you mean: 

ST10 Flasher interface & Connection.

gontsov
Associate II
Posted on August 21, 2009 at 15:11

ST10 Flasher interface & Connection.

#st10-dump
12 REPLIES 12
gontsov
Associate II
Posted on January 19, 2009 at 14:52

I have tried the 2nd MCU on this ECU, but all the same. Maybe it's require another software protocol which can start from the 0x86 responce?... Or not?...

Or there are any tricks to activate sBSL and read flash?...

[ This message was edited by: gontsov on 20-01-2009 06:39 ]

toninho
Associate II
Posted on August 21, 2009 at 15:11

This interface can be used on other processors? example. St10f168-q, 272,280; automotive line? If so could i inform other models?

algontsov
Associate II
Posted on July 06, 2010 at 21:21

Of course, this tool can flash any ST10 due to the same init commands.

But it's can't dump the flash, even if port and monitor are fine:

*Dump-->ERROR

Description: LoadExternalFlashMonitor: target Not found

Only a writing of the hex-file is possible.

Anybody knows how to start a flash dumping using this tool? Maybe it's just prohibited by ST policy or smth wrong there in the soft...