2005-10-04 04:26 AM
2005-10-04 03:15 AM
Hello, I am using an evaluation board with the STR710 microcontroller. For evaluation reasons I am running my programs from the SRAM memory which is 64kbyte. Till now no problem.
However I made a new program that is 95kbyte in size, I did not try it yet, but I think it is not possible to load into and run it from the SRAM now? I can use the flash memory which is 256kbytes, but is it debuggable? Jimmey