2008-01-14 04:39 AM
2008-01-07 07:52 AM
hello everyone! i am currently looking into using the SPI port on the STR712FR2T6 part. i noticed that the SSN pin is always show as pulled HIGH when the uC is the Master. am i to assume that this SSN pin cannot be used as a PORT0 output pin? It cannot be used as the chip select to an SPI EEPROM? so its wasted during Master mode? thanks for any info.
Bob Zeranski2008-01-14 04:39 AM
The SS on the master must be deasserted high :o You have to use another GPIO pin drive the EEPROM chip select line .
Chris.