2020-10-28 07:26 PM
Hi,
I'm trying to develop using the M24M01 product. There is a part in DATASHEET that I don't understand, so I leave a question.
In the item 'Maximum Rbus value versus bus parasitic capacitance Cbus', it is stated that the Rbus X Cbus value should come into the below time line. But if the cbus value or rbus value is too small,(ex. Rbus X Cbus = 10ns for 1kohm, 10pF) What could be the problem?
In addition, a pull-up resistor is not required on the SCL line? (Not in DATASHEET)
2020-10-29 02:22 AM
Hello,
No problem with low R x C bus. Moreover, it depends on the frequency the application operates. ( To High RxC bus will not allow 1MHz frequency )
About the pull-up resistor on SCL, ST doesn't recommend to put a pull-up resistor (even if I2C spec UM10204 does).
The application note AN2014 available on ST.COM will help you on this point. (https://www.st.com/resource/en/application_note/cd00042024-how-a-designer-can-make-the-most-of-stmicroelectronics-serial-eeproms-stmicroelectronics.pdf)
BR
Team EEPROM suPPort
2020-10-29 06:29 PM
-
2020-10-29 06:30 PM
Hi,
Thank you for your quick reply. I have an additional question.
You said that the low R X C bus has no problem. I also checked the Application note "AN2014".
Then how about not having Cbus at all? Isn't that any problem?
I look forward to your reply.
Thanks.