Skip to main content
jagauthier
Associate III
February 12, 2023
Question

printf and float

  • February 12, 2023
  • 10 replies
  • 11070 views

So, I'm having an issue getting the printf() function suite to work with floating point values.

First, understand that I am not using STM32CubeIDE. It's a good tool, but I've had too many issues/complications using it. I use a custom Makefile and VScode for my development environment.

That said: With STM32CubeIDE I *can* go into the options and select "Use float with printf from newlib-nano (-u _printf_float)"

This adds "-u _printf_float" to the linker flags and floating point values work.

In My Makefile, I've added "-u _printf_float" to the linker arguments and floating point values are always "0.0".

I'm not sure what else would be causing this.

STM32's linker line versus mine:

arm-none-eabi-gcc -o "CT_ReadG431.elf" @"objects.list" 
-mcpu=cortex-m4 -TSTM32G431KBTx_FLASH.ld
--specs=nosys.specs -Wl,-Map="CT_ReadG431.map" -Wl,--gc-sections -static --specs=nano.specs
 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -u _printf_float -Wl,--start-group -lc -lm -Wl,--end-group

Mine:

arm-none-eabi-gccm [Object list omitted for brevity] -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard
 -specs=nano.specs -TSTM32G431KBTx_FLASH.ld -lc -lm -lnosys 
 -Wl,-Map=build/CT_ReadG431.map,--cref -Wl,--gc-sections -u _printf_float 
 -o build/CT_ReadG431.elf

Could it be something else?

This topic has been closed for replies.

10 replies

KnarfB
Super User
February 12, 2023

Try to match the order of the flags as close as possible, e.g. put it between nano.specs and the linker script.

hth

KnarfB

jagauthier
Associate III
February 12, 2023

Thanks for that. I did try that without any added success. What solved it was implying I did not want any form of optimizations (-O0)

I can reliable break and fix it by adding (or removing) compile time optimizations.

waclawek.jan
Super User
February 12, 2023

> In My Makefile, I've added "-u _printf_float" to the linker arguments and floating point values are always "0.0".

I don't use printf() in microcontrollers, but my understanding is, that it the float printing is off, then it won't print anything, i.e. not even "0.0".

JW

jagauthier
Associate III
February 12, 2023

That was also my understanding. I resolved this by enabling -O0. Whenever optimizations are enabled in the compiler all values are 0.0.

KnarfB
Super User
February 13, 2023

@Community member​ is correct.

printf("temperature: %4.2f [C]\n", temperature);
 
temperature: 22.38 [C] <-- linked with -u _printf_float
temperature: 22.44 [C]
temperature: [C] <-- linked without -u _printf_float
temperature: [C]

The "-O0 is healing" looks more like a missing volatile or issues with using floating point in interrrupt handlers or similar syncronization issues.

hth

KnarfB

S.Ma
Principal
February 14, 2023

I try not to use float as it's adding float libary to flash footprint.

You can make your own printf function with your own tags for formatting.

If float is to show something like " 29.375",

uint32_t temp_degC_x1000 = 29375;

MyPrintf("temperature is %M degree Celcius", temp_degC_x1000);

Example of custom printf :

void LCD_16x2_Printf(LCD_16x2_t* pL, const char *str,...)

found in LCD_16x2.c file here