cancel
Showing results for 
Search instead for 
Did you mean: 

Sector 0 in FLASH program memory (ST7LITE2)

hkurt
Associate II
Posted on May 20, 2004 at 11:46

Sector 0 in FLASH program memory (ST7LITE2)

2 REPLIES 2
hkurt
Associate II
Posted on May 18, 2004 at 13:22

Can anybody tell me for what this special sector is (it has to be setup in the Option Byte).

If there is somewhere a decription pls specify where I can find it.

Kurt

itsmejatinus
Associate II
Posted on May 20, 2004 at 11:46

The Sector 0 can be used for in-application programming(IAP). The reset and interrupt vectors are located in Sector 0. Pls also refer ''flash programming manual'' . It can be downloaded from the same site.