cancel
Showing results for 
Search instead for 
Did you mean: 

reset the timers

adi2
Associate II
Posted on November 24, 2003 at 13:51

reset the timers

5 REPLIES 5
adi2
Associate II
Posted on November 24, 2003 at 12:01

hi !

when i use the output compare function , when i'm writing to the CLR register will it reset the counter ????

thanks.

adi
jatin
Associate II
Posted on November 24, 2003 at 12:08

Which device are you using??

adi2
Associate II
Posted on November 24, 2003 at 12:17

st72264

jatin
Associate II
Posted on November 24, 2003 at 12:56

Yes, while using 16-bit timer/output compare function , the counter is reset by writing into the count low register(CLR). It is also mentioned into the datasheet.

adi2
Associate II
Posted on November 24, 2003 at 13:51

yes ,it is written in the datasheet but not under the output compare function section and i just wanted to be sure.

thanks.