2005-02-09 08:43 AM
2005-02-02 10:09 PM
Is there anyone that has already and successfully an OS ported to STR71x target ?
If yes, what is the OS's name ? and what are the tools used ? Thank you2005-02-02 10:34 PM
Hi,
if i can add... RTOS with TCP/IP functionality...2005-02-03 02:25 AM
Hello OneR,
We have already did this with a uClinux OS . An application note,which describes how to port a uClinux on STR71x package, will be published soon. Regard, Hich :p2005-02-03 02:19 PM
We have already ported uC/OS-II to STR71x.
Our customer is using the OS for a STR710 application2005-02-03 07:45 PM
Hi Zouh,
I'm really interested in your ucLinux port. For the uc/Os II, is it an official port ? Best regards2005-02-03 10:02 PM
Will these ports (uCLinux / uc/Os II) require any external RAM/ROM or will the internal memory be enough?
/Beach2005-02-03 10:41 PM
I have ported FreeRTOS to the str7, not a full rtos but small scheduler - ok for smaller 711/712 devices.
Regards sjo2005-02-09 08:43 AM
Hi sjo,
interested in the FreeRTOS port you made. Do you make it public ? Regards, CeeCee