2020-06-04 04:41 AM
Hi Team,
I am working with ST10F276E Micro controller being MDK-arm not supported installed C166 toolchain eveluation version and it was successfully build.
My question that i want to download the code into flash (microchip IC) i found something like
JTAGjet-166(http://www.keil.com/dd/chip/3545.htm)its with IAR embedded workbench.
So, is there any flash utility to support downloading the hex file into the flash using UART calble or any ST-link/u-link debugger(JTAG) to purchase..???
Kindly suggest.. 🙂
2020-06-04 05:41 AM
Like ST10 Flasher?
2020-06-04 05:46 AM
hope u got my question i mean to say do i no need to use any STlink debugger (adapter) as interface to pc and board (if need to use i dont have connection setup at boradside) so directly thrpugh UART interface can ST10 flasher will work...????
2020-06-04 09:07 AM
You're using an obsolete device. What active support there used to be has moved on.
I'm answering the question : "So, is there any flash utility to support downloading the hex file into the flash using UART cable"
Yes, there's a tool called ST10 Flasher that does exactly that.
Not sure how well it handles COM ports with high indicies, really OLD software.
https://community.st.com/s/question/0D53W000004lNH9SAM/how-can-i-get-the-st10-flasher-tool