2008-02-28 03:24 AM
Problems with the breakpoints in the debugger of the uVision2 & 3!!
2011-05-17 02:52 AM
When I try to emulate a program with several banks with the debugger of uVsion, if I put a breakpoint in a code line of the any interrupt routine (link on common area), the debugger doesn't stop. The program is executed correctly.
Does somebody know which is the problem? Do I need configurate any parameter in the uVision? Thanks for your help, Miguel