2003-09-01 06:52 PM
2003-08-21 01:33 AM
Hi,
I have problem programming the NMI pull-up on ST62T32B with winee 4.0.2 When I set 'D2 NMI pin pull-up enabled' to 1 (ON) there is no pull-up present on the NMI pin. But if I set 'D2 NMI pin pull-up enabled' to 0 (OFF) and 'D3 TIMER pin pull-up enabled' to 1 (ON) there is a pull-up on the NMI pin !! It seems to me that the bits D2-D3 are mixed up. Am I right or is it my brain thats mixed up? Regards Bood2003-09-01 06:52 PM
You are right, D2 and D3 Bits are explained reversed in the datasheet. In Actual , bit D2 is used to pull up Timer pin and D3 to pull up NMI Pin.
The datasheet will soon be modified accordingly. Thanks for your help.