2019-08-18 03:04 AM
Where can I get datasheets and manual on this MCU : ST10F296M-A1 ?
Further numbers on it: VG023240 992DH MYS 22 035
Closest I found was a doc CD00211833, ST10F296E (which seems like, a device user manual?)
And nothing else with the exact number is printed on that chip.
Anyone ..?
2019-08-18 12:33 PM
Try alldatasheets.com like website, they are sticky with specs which survive the NRND/Product Termination phase.
(which is good for maintainance people I would guess)
Example of datasheet at distributor's
https://www.mouser.in/datasheet/2/389/stmicroelectronics_cd00010672-1205484.pdf
2019-09-03 10:59 PM
I saw that before, but that is wrong model number.
The closest I saw was ST10F296E
2019-09-03 11:09 PM
Although, alldatasheets.com does have which is probably the one there is really.
https://www.alldatasheet.com/view.jsp?Searchword=ST10F296M
Seems that the "M" or "E" at the end differ in flash size, while the "-A1" probably is the dimension package variant of PBGA.
May be that ST10F296E datasheel/user manual the only one there is.
Thank you