cancel
Showing results for 
Search instead for 
Did you mean: 

Minimum Voltage for Operation

paulbrown9
Associate II
Posted on July 14, 2004 at 09:49

Minimum Voltage for Operation

1 REPLY 1
paulbrown9
Associate II
Posted on July 08, 2004 at 13:47

The evaluation board schematic shows the use of a 2.63V STM811 supervisor circuit for providing a reset pulse.

However the Datasheet for the STR71X says the minimum operating voltage is 3.0V and that ram retention is only guranteed above 2.7V when in low power mode.

Should a supervisor circuit be 3.0v rather than 2.63v or is the datasheet incorrect.

Cheers