cancel
Showing results for 
Search instead for 
Did you mean: 

M25P64-VMF6G The above part number was belongs to STM or Micron, Some of the datasheet show it was STM and some are Micron.

VVelu.1
Associate
 
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @Community member​, to the community!

You are currently talking about an very old serial flash memory, which was spun off with the entire business unit in 2007 to the company Numonyx, which in turn was subsequently taken over by Micron. Unfortunately, STMicroelectronics cannot say what the successors did with this memory device.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @Community member​, to the community!

You are currently talking about an very old serial flash memory, which was spun off with the entire business unit in 2007 to the company Numonyx, which in turn was subsequently taken over by Micron. Unfortunately, STMicroelectronics cannot say what the successors did with this memory device.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.