cancel
Showing results for 
Search instead for 
Did you mean: 

TCXO on STM32WL33

GScha.1
Associate II

Hello,

 

I would like to know if it possible to use a 48MHz TCXO instead of the 48Mhz crystal specified in the datasheet of the STM32WL33 ?

Standard crystal are at minimum +/- 10ppm at tolerance and this may not be sufficient for our application.

 

If yes, do I left the OSC_OUTPUT in floating ?

 

Best regards,

 

Schaeffer G.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Uwe Bonnes
Chief

Of course it is possible. But you need to enable LSE bypass. Read the docs how to do so. Osc_OUTPUT can be reused, with the restriction of the PC13-15 restrictions.

View solution in original post

1 REPLY 1
Uwe Bonnes
Chief

Of course it is possible. But you need to enable LSE bypass. Read the docs how to do so. Osc_OUTPUT can be reused, with the restriction of the PC13-15 restrictions.