2005-02-25 11:00 PM
Locating absolute segment (program/constants) using the STVD7 3.0
2005-02-25 11:28 AM
Using the STVD7 3.xx we tried to locate an absolute segment at sector 1 of 72F521N9 with no success.
Using STVD7 2.54 this was done with the following command: # locate .e4dTP1 at -b0xe000 +seg .e4dTP1 -b0xe000 -n .e4dTP -m4096 d:\sw\e4Gen\object\T4cons.o How can I do that using STVD7 3.xx? Any syggestions anyone?2005-02-25 11:00 PM
similar method, you need to overide the generated linker script via project settings/linker input and uncheck the auto checkbox.
modify script as you did in the older version. Regards sjo