2007-01-16 08:12 PM
Is there IAP example code available?
2011-05-17 12:35 AM
I need program Bank0 from Bank1.
WBR, Dawei Shang2011-05-17 12:35 AM
Hello shangdawei,
Yes, ST will provide a driver allowing programming the STR91x Internal Flash Bank0 using In Application Programming via UART. The IAP driver is to be programmed by the user in the Flash bank 1 after being hardware remapped at address 0x00 (bank 0 is hardware remapped at address 0x80000). Programming is performed via JTAG using a flasher toolset. Using the UART, the IAP driver loads a binary file from HyperTerminal to the STR9 internal Flash bank 0, and then jumps to execute it. More details will be provided in the ''STR9 In-Application Programming using UART'' application note which will be published on the web few days later. Best regards, Najoua.2011-05-17 12:35 AM
Hello again shangdawei,
Now, the ''STR9 In-Application Programming using UART'' application note (AN2475) and its corresponding software are available on the following web link: http://www.stmcu.com/modules.php?name=mcu&file=familiesdocs&FAM=101 Best regards, Najoua. :-P