2007-02-08 11:23 AM
In circuit bootloader via RS232 or USB ?
2011-05-17 12:30 AM
any news about the source files for the DFU ?
2011-05-17 12:30 AM
use STR750F
2011-05-17 12:30 AM
Any news on the boot loader ?
2011-05-17 12:30 AM
Hi
I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space. Best regards Vendelin2011-05-17 12:30 AM
Hi
I read pdf file about UART bootloader and I have one question. Is the start adress of bank 0 after remaping by CAPS 0x80000 or 0x8000? Bank1 has only 32kB adress space. Best regards Vendelin2011-05-17 12:30 AM
Hello Vendelin,
Bank0 is remapped to address 0x80000 using CAPS and Bank1 size is 32Kbytes as you said. Regards, Najoua. [ This message was edited by: Najoua on 07-02-2007 09:57 ]2011-05-17 12:30 AM
I was just reading an article in embedded-Developer.com. Here is the link.
http://www.embedded-developer.com/tools/470/STMicroelectronics/um0290.htm It says that the USB Boot loader called a DFU. What does DFU stand for? Is available in the USB developer kit. I haven't checked it out yet but it is something I need for my project. :-D2011-05-17 12:30 AM
Hi All,
Will This bootloader work for STR912FAW46 ? Regards Sai2011-06-28 12:44 AM
Where is the link to download?
2011-06-28 11:47 AM
Where is the link to download?
AWOL The thread is from 2006/2007, a prior incarnation of the forum, and user database. The current forum had a meltdown in mid May 2011. Attachments have not survived these processes, ST might be able to dig them out of the archives, but that's not certain. You may want to check if the material is mirrored other places on the net, or that the posters are active on other forums.