2004-07-13 07:37 PM
How to restore RC calibration values
2004-07-12 05:19 AM
I need to set the readout protection after programming and calibrating the RC. If I reprogram the device, reset the read-out protection. Then the whole memory including the calibration values (RCCR0 and RCCR1) are erased. How can we restore these values?
2004-07-12 05:52 AM
Which MCU are you using?
Which in-circuit programmer are you using?2004-07-13 12:01 AM
I am using MDT10 EPB for programming.
The device is ST72FLite292004-07-13 12:10 AM
When you are programming the device using STVP7 1.9.2. Then the RCCR values will be restored by itself. The programming mode selected should be either “Socket� or “ICP OPT Disable�.
2004-07-13 07:37 PM
Thanks for the information