2006-12-07 05:24 AM
2011-05-17 12:34 AM
Yesterday I started using the CAPS tool (ver 2.30) for an STR911FM44 with the stdlib code. I have the include files and paths all set up correctly. However, I get about 20 unresolved variable errors when I compile 91x_conf.c. The errors have to do with pins which are not found on the 80 pin package (ports 0, 1, 7, 8, 9, etc.).
Is there a version of 91x_conf.c for the 80 pin package or do I need to manually edit the one I downloaded? Thanks for any help which you may be able to provide.