2009-03-21 10:08 PM
First problem solved, new one to fix!
2009-03-21 10:08 PM
I've solved my first problem! As I was migrating from SOFTEC InDart with specific STVD7 to RAISONANCE R-Link with standard STVD7, I get a lot of trouble because of the settings! In fact I was not using the right s19 file! Now I can program but still not debugging! I've to spend time to read the ST help files!
New problem, I'm discovering ST7FOX and it's specific features, for example the pull-up inputs that comes mandatory with an interrupt! I've do my hardware as if I was using ST7LITE19 so no hard pull-up! 2 solutions : 1- I place pull-up resistors (difficult on my card already existing and very compact) and I set inputs as floating inputs whitout interrupt! 2- I find the way to disable external interrupt by software but keeping the Lite Timer interrupt (I use it to create a time base)! If someone have any idea on how to do that with the FOXK1 you're welcome! Regards whitebull